Other Parts Discussed in Thread: PCM1861, PCM1821-Q1, PCM1821,
Tool/software:
Hi All,
I'm using PCM1861 ADC with H/W conorl mode and I2S format by connection 12.88MHz OSC as below to make a default 48KHz Fs rather than 24.576MHz Crystal. It's located close enought to IC

But sometimes, there is not working situation so when putting a few pFg(18pF) to C22, C25 wihout Crystal, this situation has been disappeared..
Previoulsy, I used 24.576MHz crystal with this 18pF and I never encoutered this one..
In PCM1861, is it having some weak point when using 12.288MHz OSC? If so, is it OK to put a few pF like above without crystal? Help to get your advice
By the way, I'm using alos PCM1821-Q1 together with putting 12.288MHz OSC but in PCM1821, it's working well without such an issue.
Help to get your suppotting to identify it
Thanks
Best regards,
Jaydon
Best regards,
Jaydon