TAS2563: How to get started

Part Number: TAS2563
Other Parts Discussed in Thread: , PPC3-EVM-MB, PP-SALB2-EVM

Tool/software:

Hi team,

Could you help below to TAS2563 and customer would consider to run for their new project?

Thanks!

1. For in-system tuning, is HW connected structure as below, right? 

PC(install PPC3 SW) -->  PPC3-EVM-MB --> TAS2563YBGEVM-DC --> connect to customer's PCB board

2. For in-system tuning, which pins customer should connect to TAS2563YBGEVM-DC?

3. To protect amplifier and  run in-system tuning, need below EVMs, right?

EVMs

Application

PP-SALB2-EVM + TAS2563YBGEVM-DC

Learning amplifier to build parameters to protect amplifier

PPC3-EVM-MB + TAS2563YBGEVM-DC

1. Adjust parameters even no connect to customer's PCB board

2. Run in-system tuning when connect to customer's PCB board

4. When adjust done, will get a cfg file, right? And how can customer implement in their project SW? 

5. Also anything I miss above?

Thanks!

  • Hello,

    Is the customers application an android based system? This will alter the response to your questions. Slight smile

    Regards,
    Sydney Northcutt

  • Hi Sydeny,

    Please see the reply from customer in below.

    No, it is not an android-based system.

    We do not have any OS in our system. Thanks.

  • Hello,

    1. For in-system tuning, is HW connected structure as below, right? 

    PC(install PPC3 SW) -->  PPC3-EVM-MB --> TAS2563YBGEVM-DC --> connect to customer's PCB board

    Yes, for in system tuning without an android based system both the PPC3-EVM-MB and TAS2563YBGEVM-DC will be needed and connected to the PPC3 software. To do the in system tuning, bring out the I2C pins from the device on the end equipment and connect them to the TAS2563YBGEVM-DC. The only thing you will need to do is disconnect the device that is on the EVM so only the device on the end equipment is recognized and controlled. 

    2. For in-system tuning, which pins customer should connect to TAS2563YBGEVM-DC?

    The customer should bring out the SDA and SCL pins on their system and connect them to the EVM. 

    3. To protect amplifier and  run in-system tuning, need below EVMs, right?

    Correct. Speaker characterization should be done with the EVM though, not with the in system device. For speaker characterization the following document can be referenced: https://www.ti.com/lit/ab/slaa952/slaa952.pdf?ts=1733935700070&ref_url=https%253A%252F%252Fwww.ti.com%252Fproduct%252FTAS2563

    After the speaker has been characterized, they can then move to in system tuning. 

    4. When adjust done, will get a cfg file, right? And how can customer implement in their project SW? 

    Yes when tuning is finished they can save configuration and header / binary files to use in their SW. 

    Regards,
    Sydney Northcutt