Other Parts Discussed in Thread: PCM5142,
Tool/software:
Hi All,
Is the 10uF electrolytic capacitor on the LDOO pin necessary?
Also, if possible, can I change the electrolytic capacitor to a ceramic capacitor?
Best Regards,
Ishiwata
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
similar to any other supply voltage you want to use the decoupling capacitor on LDOO as well, so you should not skip them.
The users guide has the recommended cap types and values , which are used on the EVM as well. In general one should stay with those recommendation , but if one needs to replace a component due to some constraint, it should be ok.
Regards,
Arash
Hi Arash,
Thanks for your answer.
For example, the circuit diagram in the datasheet for the PCM5142 lists the 10uF electrolytic capacitor as DNP, so I wondered if the PCM5101A could also be DNP.

Could you please tell me why the PCM5142 is DNP?
Best Regards,
Ishiwata
Hello Ishiwata,
It all depends on supplies and board. In the EVM schematics, all 10uF are DNP, seems there is already good stability for those supplies (there is a 100uF connected to the 3.3VA supply switches.) So on the EVM, they DNP all the 10uF caps at the pins including LDOO. Since with only 0.1uF LDO's stability is fine, I don't see any issue with leaving 10uF out for this case.
Regards,
Arash