This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM4222: Interference Issues in Multi-PCM4222 Applications

Part Number: PCM4222

Tool/software:

Hi,

I have designed a functional test (FT) board using the PCM4222, with a total of 4 sites, each equipped with one PCM4222. I’ve encountered an issue where using the ADCs simultaneously causes interference between them. The main problem is the appearance of low-frequency noise, leading to ADC output not meeting expectations. When only one site is active and the others are turned off, the tests perform normally.

Could you suggest potential approaches to improve this situation? Would you recommend adding more LDOs to isolate and prevent power supply interference? The analog/digital interfaces for different sites are independent. Could this be a clock interference issue affecting the ADC and causing aliasing problems as well?

Thank you.