Part Number: TAS5822M
Tool/software:
Hello, TI Team
I am not sure if I can communicate well because my English is not good enough, but thank you in advance.
When the speaker is not connected and white noise is sent via I2S, if the POWER_STATE register (offset = 68h) is set to Play state, OTSD_I in the GLOBAL_FAULT2 register (offset = 72h) will be set to '1'.
If OTSD_I is not set to '1', OTSD_I remains '0' no matter how many minutes of playback are performed.
This happens after power-on.
When OTSD_I is set to '1', the device instantly becomes hot.
Even if I reset the OTSD_I flag in software, OTSD_I is set to '1' again immediately.
Are there any possible causes?