Part Number: DRV2700EVM
Tool/software:
Hi,
I want to vary the output voltage linearly (0V to +105V) in single ended DC input with set reference configuration, I have followed the steps mentioned in the DRV2700EVM user guide (SLOU403C) section 5.4.1, but the output voltage is non-linear with respect to the input DC voltage (0V to 5V) applied at pin TP7(IN+), with DC reference input at 2.5V applied on pin TP8(IN-).
Steps I followed:
- Removed jumpers JP6 and JP5
- Connected EN, GAIN0 and GAIN1 jumpers to PU as to enable the driver and config the gain to 40.7db
- Connected DC reference 2.5V to TP8(IN-) pin
- Connected a variable voltage source (0V to 5V) to TP7(IN+)
- Disconnected jumper JP_DC and powered the evaluation board with external power supply applied to J2 terminal
- Measured voltage with a multimeter between pins OUT+ and GND
Observations:
- As soon as powered up and with input 0V applied at TP7(IN+) the output voltage is 1.62V but not 0V
- from 0V to 1.6V input the output voltage is constant at 1.62V, no linear change
- from 1.7V to 3.5V input voltage the output seems to be jumping randomly from 6.25V to 103.2V, not following a constant gradient change
- from 3.6V to 5V input the output voltage is saturated to 103.2V, not reaching till 105V
Can you help me figure out where have I went wrong how to configure the DRV2700EVM to properly operate it linearly, is the amplifier after the boost converter a rail-to-rail amplifier or not?