Part Number: PCM1809
Tool/software:
Hi team,
I have a few questions.
- In Figure 7-1, capacitors with and without polarity are written separately.
Should I use polarized capacitors where it says polarized? - I am aware that the capacitor capacity for the quick charge scheme function can only be set to a maximum of 1uF.
If AC coupling is done with a capacitor larger than 1uF, will the quick charge scheme not work? - Can I use Left-Justified?
The datasheet describes the switching characteristics of LJ, but I think the Mode is TDM or I2S.
If LJ can be used, is there anything we should pay attention to? - Is the only difference between controller mode and target mode the clock configuration?
Are there any advantages or disadvantages to using each?
Best Regards,
Ryu.