Tool/software:
Hello, good morning!
I need a help whit TPA3255 (Schematic ZK-3002).
I would like some technical information about the TPA3255.
Here is the layout scenario:
Four amplifiers (TPA3255 (PBTL MODE) (ZK-3002)) with their inputs connected to
the same output of a preamplifier, and all amplifiers (TPA3255) are connected to
the same 24VDC power supply.
In an isolated test (single amp PBTL MODE) with 24VDC power supply, it was able
to supply 12A AC at 60Hz with a load of 1 OHM (THD <1.2%).
However, when connected and operating with other amplifiers,
and the negative power output ((- NEG. TPA3255) (PBTL mode)) of the amplifiers
is connected to a common point on the negative of all, oscillations and faults
occur.
When turning on the system without a signal or load, you can hear some clicking
noises in the inductors, and the FAULT signals remain pulsating (+ to GND) while
the (- NEG. TPA3255) connections are connected.
If you remove the (- NEG. TPA3255) connections, the problem stops. However, I
need these connections to always be active in the layout.
After testing, it was found that with an independent power supply (one source
for each amp without even sharing GND), the faults no longer occurred and the
system operates normally.
I would like to know how to use this configuration, 4 TPA3255 amplifiers
operating with a common output (OUT -) and the same DC power supply.