Tool/software:
what are the frequency for high pass filter.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Our codec expert is out of office until Tuesday. Please be patient as responses will be delayed
Hi,
Are you talking about the input high pass filter? It is given by the equations below:
Fc = 1/(2*π*Req*Cc)
Cc = 1/(2*π*Req*Fc)
For high fidelity audio recording application it is desirable to keep the cutoff frequency of the high pass filter as low as possible. For single-ended input mode, the equivalent input resistance Req can be calculated as:
Req = Rin* (1 + 2g)/(1+g)
The variable g is the analog PGA gain calculated in linear terms:
g = 10000 * 2floor(G/6)/Rin
where G is the programmed analog PGA gain programmed (in dB) and Rin is the value of the programmed input resistor
and assumes Rin = Rcm.
Best regards,
Jeff McPherson
Dear Sir,
Audio requirement details are as given below-
Signal name : Audio signal
Signal type : Analog stereo
Frequency : 300Hz to 3.5 KHz
Signal voltage : 0.4 to 5Vrms across 10K
Input impedance : 10KΩ
No of channels : 2
Hi,
The minimum input impedance of the device is 20kOhm. Is that acceptable?
Thank you,
Jeff McPherson