This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA2026D2: TPA2026D2 - 3W, 4ohm Stereo speaker integration, Reference design

Part Number: TPA2026D2
Other Parts Discussed in Thread: TPA2017D2

Tool/software:

Hi,

I’m using the TPA2026D2 audio amplifier in the output section along with the WM8904CGEFL/V codec, and planning to drive two 3W, 4Ω speakers. Could you please confirm if this amplifier is suitable for such an application?

In the EVM schematics, I noticed that it mentions support for 8Ω to 32Ω speakers. Could you clarify whether 4Ω speakers can be supported in this setup? If not, please suggest an alternative amplifier suitable for driving 3W, 4Ω speakers.

Additionally, it would be helpful if you could share any available reference design files for our application.


Best Regards
Akin