This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS2X63EVM: Not showing as an audio output in windows but I can connect with PPC.

Part Number: TAS2X63EVM


Tool/software:

The EVM intermittently shows up as an audio device on my windows 11 PC and I am usually unable to use it as an audio output on our PC, stalling development. 

The EVM does connect with PPC. 

The EVM is powered by a 5.5v supply. Attached is a photo of the EVM, possible there are incorrect jumper positions?

- Sometimes there is no audio output

- After restarts and power cycling, I see the speaker flash rapidly in the windows task bar

- Rarely, it will connect properly. 

I've swapped USB cables and power cycled our PC and EVM. 

Windows 11

I've included screenshots for more context. 

Thank you.