Part Number: DRV5825P
Other Parts Discussed in Thread: TAS5815, TAS2572, TAS2781, TAS2780
Tool/software:
Hi Team,
Do we have mono piezo driver supporting I2S input? I only found DRV5825P stereo solution. Thanks.
Best regards,
Terry
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Terry,
You can technically use other Class-D digital input amplifiers, such as TAS2780/TAS2781 or TAS2572 to drive a piezo actuator. In any of these cases you must add an LC filter with proper saturation current (usually at least 4A) and a current limiting series resistor in the order of 3~4Ohms to avoid OCP trigger.
For the devices with speaker protection algorithm integrated, this feature must be disabled as it is intended only for dynamic/conventional speakers.
Best regards,
-Ivan Salazar
Applications Engineer