Part Number: TAS5782M
Tool/software:
Hello,
We have designed a PCB around the TAS5782M, the I2C lines are common between the TAS5782M, a 512kb EEPROM, and an STM32.
Now using the PPC3, and after setting our customized parameters, we would like to upload the settings and flash it on the EEPROM, in order to have a standalone operation, so that the TAS5782M can selfboot from the EEPROM without using the motherboard again.
The second question is, how to get the hex file from the PPC3, and in what format, and how to flash this file on the EEPROM.
The third question is, Does the TAS5782M need to be configured to pull the data from the EEPROM by itself or does the STM32 need to orchestrate the data flow between them and how - a detailed answer is appreciated.
Best Regards.