Tool/software:
Hello
please tell me if the mentioned power in the data sheet is RMS , PEAK , AVERAGE ???

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello
please tell me if the mentioned power in the data sheet is RMS , PEAK , AVERAGE ???

for example:
when input increase, the amp's output voltage also increase.
when thd = 1%, the output voltage can get A vols. here the A usually means rms value. the peak voltage is A*sqrt(2).
then we use A^2/Rload = power.
this power is what we listed in above DS.
generally, power use the Vrms to calculate.
if there are special description peak power, then here might use peak voltage to calculate the power.
so what exactly your rms and peak means?