This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS6754Q1EVM: The frequency response on the low frequency side has dropped by about 0.1 dBV.

Part Number: TAS6754Q1EVM


Tool/software:

When measuring the frequency response with Audio Presicon, CH1 and CH3 showed a drop of about 0.1 dBV in the low frequency range.
(The FR of CH2 and CH4 is flat.)

<Question>
Do you know the reason why CH1 and CH3 showed a drop of about 0.1 dBV in the low frequency range?
Please advise on what to check in order to make it flat.

<What I checked>
• Replaced the AP measurement cable.
• Replaced the 4-ohm resistor.
• Replaced the cable between the EVM board and the 4-ohm resistor.

<Test Conditions>
• The PPC3 and register settings are set to default.
• PVDD = 14.0V
• A 4-ohm resistor is connected to the OUT terminal.
• Audio data is input to the EVM board from the AP via optical connection.
• Normal output is confirmed from CH1 to CH4.