This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM9211: Configuration issues of PCM9211

Part Number: PCM9211


Tool/software:

Hi ti team,

Excuse me, can the PCM9211 be configured to have 1 channel of SPDIF input and 2 channels of SPDIF output simultaneously?

  • Hello,

    Yes in datasheet it mentions:

    There are two S/PDIF outputs available in the MPO port; MPO0 and MPO1 output can be selected independently. The MPO pins are also able to output DIR flag information, interrupt flags, or to repeat S/PDIF signals selected for the RECOUT0 or RECOUT1 paths.

    Kind regards,

    Arash