Other Parts Discussed in Thread: TAD5242
Tool/software:
Hi TI Experts,
I'm currently evaluating the TAD5242EVM-K and have connected an external I2S source to the AC-MB board included in the evaluation kit.
My MD0–MD5 configuration is as follows:
-
MD0 – Shorted to ground (I2S Target Mode)
-
MD1, MD2 – Set to
2'b10-
AVDD = 3.3V
-
Word Length = 24-bit, Linear Phase
-
Decimation/Interpolation enabled
-
-
MD3 – Set to
1'b0(Quick Charge enabled) -
MD4, MD5 – Set to
2'b00(DAC Diff LO – Highest Performance) -
MD6 – DOUT1 = jumper header to GND
However, when I probe the output signals using an oscilloscope, I’m not seeing any signal from OUT1P and OUT1M test points. Additionally, OUT2P and OUT2M are producing identical waveforms, resulting in a flat line at 0 when using the math function. Moreover, the MD0-MD6 configuration settings on the TAD5242EVM-K user guide is different from the ones on the TAD5242 datasheet.
I have also taken a look at TAD5242EVM-K: Only one channel has sound. . I have checked over and over again, but I kept getting the same result
Is there a configuration step I might be missing? Would you be able to share the correct jumper header settings for the board, or confirm if this setup works on your end?
Thanks in advance for your support.
Best Regards
Ena