Hi,
I bought the EVM for the above device to evaluate it's suitability for a transducer amplifier for underwater acoustics. The frequency band of operation is from 16khz to 35khz. According to the data sheets the device is capable up to 80 khz. I coupled the evm to the transducer via a 1:20 isolation transformer to match the impedance between the amp and the transducer. The transducer has an impedance of about 2koms.
I was expecting plenty of acoustic power out but I was dissapointed to find out that I can only increase the input amplitude from 0 to 10% of full amplitude and the power output is no more than a couple of watts. Any more increase in the output power puts the device into fault condition and has to be reset. The transducer element is a piezo ceramic ring with around 9nf capacitance.
We have been using the TPA032D01 for years in this application successfully. The TPA is a much smaller device that the TAS5611A therefore I expected much greater power output at least up to 50-60W. I also looked at waveform on the secondary of the transducer by connecting it to an oscilloscope. I found that as the input voltage was increased to the proximity of the threshold where the device would cut off, there were discontinuties in the output waveform with large ringing in the out put.
Can you provide some advice on what I am doing wrong? What is the cause of the ringing? Can this amplifier be used in this type of application? It would be great if we could. We are planning to sell many of these products using the TAS if it can be successfully implemented in the design.
I await your valuable comments.
Best regards
Manjula
CTO