PCM4202EVM: Board not providing output signals

Part Number: PCM4202EVM
Other Parts Discussed in Thread: PCM4202

Tool/software:

Hi,

We are trying to use the PCM4202 in DSD mode.

The power supply of +15 V, -15 V, +5 V digital and +5 V analog have been provided with internal regulation of +3.3 V (Jumper on 1 and 2).

The clock signal is not appearing at LRCK.

May i know why is this the case ?

I have attached a picture of the switch configurations set up.

Is there any other configuration missing or that has to be done ?

I request assistance in getting DSD signal at the outputs and clock.

Best Regards,

Tarun Manoj