Part Number: TAC5112
Other Parts Discussed in Thread: PUREPATHCONSOLE, TLV320AIC3204
Hello,
I'm looking at the TAC5112 - for our application we need it to run at 125ksps stereo (not a multiple of 48 or 44.1kHz).
- The PASI_SAMP_RATE[5:0] option of 128000 (111720-131840) covers this frequency so I assume it can be run at this rate?
- The filter responses in the datasheet are all at the "standard frequencies" - how do I tell which filter reponse I will be seeing at this sample rate?
- I've put in a request for PurePathConsole - will this make everything obvious?
- We've previously run a TLV320AIC3204 at 125kHz and had to use a bi-quad to gain up the channel due to the non-standard sample rate. Is there anything like this I need to think about?
Dave
What