We make Active noise reduction modules for headsets. I recently replaced our old BTL chip with your class D. Everything is fine except for a violent click on power off. The circuit is comprised of a mic preamp into a lead/lag filter that is buffered on output through a unity gain opamp. The filter and preamp are referenced mid-supply. When I had the IN- of the class D tied to battery ground (with a capacitor) there was a loud pop coming on but when I tied it to the vref this mitigated the on going click. So it is single ended input to differential output and I have payed attention to matching impedances on the IN+ and IN- of the TPA2006D1. I did have a RC delay setup on the SD pin and it worked well coming on but going off the class D did not like it so I removed it but the click did not go away....... I'm at a loss! Oh yes and the impedance of the speaker is 42 ohms and the gain is set low on the class D and high at the filter (I had it the other way but saw that you did not recommend that) I spent a day and a half reading and scanning the forum (over 1250 posts) looking for a clue but did not find it...hence the post.
Regards,
Matthew Byrd
Headsets Inc.