Part Number: TLV320ADC6140
Other Parts Discussed in Thread: PCM1690
Hello,
I am currently using two TLV320ADC6140s for my device, and I want to be able to smoothly modify the biquad coefficents without it sounding choppy and cutting in/out. The ADCs are configured for 4 channels each (8 channels total) at 96 kHz, and I have had success testing different EQ filters based on values I generated from PPC3 software.
Right now, I am powering down the ADCs through the PWR_CFG registers (also disabling inputs/outputs with IN_CH_EN and ASI_OUT_CH_EN). Once the coefficients are written, I add a short delay then power the ADCs back up. I figure this is the safest way to configure the biquads (I use a similar method for changing the input gain, which requires powering down the ADCs according to the datasheet).
However, because I am adding that delay and manually shutting down the ADCs, I can't continuously modify my EQ and get a smooth output. I have tested NOT shutting down the ADCs, but I still hear some choppiness and audio artifacts when trying to modify different parameters on the fly (I'm calculating my biquads locally).
Is there any workaround or solution to this problem? It would be great if I could test different filters by smoothly modifying the input parameters and then hear it without the audio cutting in and out.
Additional details about my setup:
- 24-bit TDM audio (formatted as 32-bit for interface with my two PCM1690 DACs)
- 24.576 MHz MCLK frequency
- DRE and AGC both disabled
Thank you!
Max