This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS2781EVM: Taking measurements of TAS2781EVM with an AP525

Part Number: TAS2781EVM
Other Parts Discussed in Thread: TAS2781

When taking measurements of the TAS2781EVM with an AP525I I am having a few dificulties....

1) What is the issue with measuring the output with a AUX-0025 attached? The data sheet says there are some issues but doesn't fully define the issue or the magnitude of the issue... (page 18 of the datasheet)

2)  Does the EVM automatically adapt to the BCLK, FRAME data rates that are applied to the EVM or do I have to set them in register values? The PPC3 TDM section doesn't provide a way to set these input parameters..

3) Since the data sheet mentions that the AP was used to test the TAS2781, is it possible to get the App Note on that work so we can verify our measured data can be correlated to the datasheet data?