Part Number: DIX9211
Other Parts Discussed in Thread: PCM9211
Hi,
All I need to do with the DIX9211 is covert an I2S signal into an SPDIF. It's massivly overkill, but I can't find anyting else that will do it. Am I looking at using the correct part?
Should I be using RXIN 0 or RXIN 2 for the input? I'm not totally sure of the hardware differences between RXIN 0 & 1 and RXIN 3-7?
Does it matter which output I use? MPO 0 or MPO 1?
I already have a 24.576 MCLK clock on the board, can I use that to drive XTI?
Will INT0 & INT1 diectly drive LEDs? All the examples I've seen buffers are used.
I'll interface to it via I2C, so I know what to do with those pins.
I don't need any clock outputs, what should I do with SCKC, BCK, LRCK, DOUT?
What should I do with all other un-used pins?
I've read on the forum to look at the ADC9211 as the part is the same (minus the ADC) and the datasheet has been updated more recently.
I've found an error in that:
In the layout example, the filter network capacitors are connected to 3V3, not GND.

Regards,
G