Part Number: TPA6120A2
Other Parts Discussed in Thread: THS6012
I was looking at some of the subtleties of the TPA6120A2 by combing the THS6012 datasheet. I came across Figure 42, Source Resistance vs Noise Factor, which is delightfully confusing.
Why is ~150R the optimal Rs for THS6012, vs anything lower?
Is the optimal Rs for TPA6120A2 also ~150R?
That graph refers to the non-inverting input, correct?
Is there any advantage (in noise terms, not offset) to matching the source resistance of the inverting input to that of the non-inverting input? For instance, in a gain of 5, one might choose Rf=402R and Rg=100R for best balance of bandwidth and peaking. But with ~150R in series with the non-inverting input, one could choose Rf=806R and Rg=200R - if it did indeed provide a noise advantage.
Thanks!