Part Number: TAD5242
Other Parts Discussed in Thread: TAD5142,
Hi team,
-
TAD5242 / TAD5142
1-1. For TAD5242 and TAD5142, is the pin named “VSSA” intended to be connected to the analog ground (AGND)?
1-2. Is the pin named “VSS” intended to be connected to the digital ground (DGND)?
1-3. For the exposed thermal pad (if present on these devices), should it be tied to AGND, DGND, or board ground in general?
1-4. Are there any specific PCB layout recommendations regarding AGND/DGND partitioning and a single-point ground connection for these DACs? -
PCM1890
2-1. For PCM1890, how should the exposed thermal pad be connected electrically?- To analog ground (AGND)?
- To digital ground (DGND)?
- To board ground (common GND plane)?
- Any restrictions about connecting the pad to noisy digital ground
Best Regards,
Ryu.