Part Number: TAS5815
Hey Sydney,
What do you recommend for the default voltage output setpoint? I understand the rail will move up and down based on feedback from the TAS5815, but I'm not quite sure where to set the default point.
Here's my understanding after chatting with an LLM:
When Class-H is OFF (disabled):
- PWM signal = LOW (ground)
- Buck-boost operates at maximum boost output
- Provides full voltage headroom you designed for
- This is the "safe" default state with maximum available power
When Class-H is ON (enabled):
No audio signal:
- PWM signal = HIGH
- Buck-boost operates at minimum boost output
- Conserves power when no signal present
With audio signal:
- PWM modulates between HIGH and LOW
- Buck-boost tracks the signal envelope
- Voltage adjusts dynamically based on instantaneous needs
I get confused (we are not using PPC3) , and do not understand the actionable next step. In my mind there would be a register in TAS5815 to define the output voltage level controlling the buck-boost. I get confused where to go from here