Hi,
After successfully using the AIC3204 in a recent project I am looking into making use of the miniDSP provided with the AIC3254. The PurePath Studio software installation provides a few examples of using the miniDSP, and it appears to generate a configuration .cfg script that may be later used to configure the AIC3254 and the miniDSP engines. I have a couple of questions regarding the AIC3254 and the generated .cfg files.
- First, the AIC3254 seems to be pin-to-pin compatible with the AIC3204. Would the current AIC3204 configuration script be 100% compatible with the AIC3254 ? If I programme the AIC3254 with the same settings as I use currently on the AIC3204 will it work without problems ? If not what changes will I need to foresee ?
 - The PurePath Studio generated configuration file for a basic process flow (from an exemple) appears to include ADC & DAC Coefficient Buffer A + B settings, when the graphical program actually includes none (as far as I know) ? This amounts to a huge number of register settings that I did not really include in the process flow ? Are these really necessary as I would prefer to keep configuration of the AIC3254 to a minimum so as to minimise application boot & start-up time. I've included a part of the generated .cfg script below.
 - As a general question, is anybody aware of a .cfg parser to convert AIC Script Language commands to C source read/write I2C commands or similar ?
 
#            --------------------------------------------------------------- page 0 is selected
w 30 00 00
#            # reg[  0][  1] = 0x01    ; Initialize the device through software reset
> 01
#            --------------------------------------------------------------- page 1 is selected
w 30 00 01
#            # reg[  1][  2] = 0xa9    ; Power up AVDD LDO
w 30 02 a9
#            # reg[  1][  1] = 0x08    ; Disable weak AVDD to DVDD connection
w 30 01 08
#            # reg[  1][  2] = 0xa1    ; Enable Master Analog Power Control, AVDD LDO Powered
> a1
#            # reg[  1][ 71] = 0x32    ; Set the input power-up time to 3.1ms
w 30 47 32
#            # reg[  1][123] = 0x05    ; Force REF charging time to 40ms
w 30 7b 05
#            --------------------------------------------------------------- page 8 is selected
w 30 00 08
#             (Bit 31-24) ------------ MSB ADC COEFF No. 0
w 30 08 00
#             (Bit 23-16)
> b7
#             (Bit 15-8)
> 98
#             (Bit 7-0)
> 00
#             (Bit 31-24) ------------ MSB ADC COEFF No. 1
> 7e
#             (Bit 23-16)
> 90
#             (Bit 15-8)
> d0
#             (Bit 7-0)
> 00
#             (Bit 31-24) ------------ MSB ADC COEFF No. 2
> 7b
#             (Bit 23-16)
> 29
#             (Bit 15-8)
> 00
#             (Bit 7-0)
> 00
#             (Bit 31-24) ------------ MSB ADC COEFF No. 3
> 84
#             (Bit 23-16)
> d7
#             (Bit 15-8)
> 00
#             (Bit 7-0)
> 00
#             (Bit 31-24) ------------ MSB ADC COEFF No. 4
> 76
#             (Bit 23-16)
> 52
#             (Bit 15-8)
> 00
#             (Bit 7-0)
> 00
#             (Bit 31-24) ------------ MSB ADC COEFF No. 5
> ff
#             (Bit 23-16)
> ff
#             (Bit 15-8)
> ff
#             (Bit 7-0)
> 00
#             (Bit 31-24) ------------ MSB ADC COEFF No. 6
> 80
#             (Bit 23-16)
> 00
#             (Bit 15-8)
> 00
#             (Bit 7-0)
> 00
#             (Bit 31-24) ------------ MSB ADC COEFF No. 7
> 7f
#             (Bit 23-16)
> ff
#             (Bit 15-8)
> ff
#             (Bit 7-0)
> 00
#             (Bit 31-24) ------------ MSB ADC COEFF No. 8
> 40
#             (Bit 23-16)
> 00
#             (Bit 15-8)
> 00
#             (Bit 7-0)
> 00
#             (Bit 31-24) ------------ MSB ADC COEFF No. 9
> 00
#             (Bit 23-16)
> 00
#             (Bit 15-8)
> 00
#             (Bit 7-0)
> 00
#             (Bit 31-24) ------------ MSB ADC COEFF No. 10
> ff
#             (Bit 23-16)
> 9e
#             (Bit 15-8)
> 00
#             (Bit 7-0)
> 00
#             (Bit 31-24) ------------ MSB ADC COEFF No. 11
> f7
#             (Bit 23-16)
> 10
#             (Bit 15-8)
> 00
#             (Bit 7-0)
> 00
#             (Bit 31-24) ------------ MSB ADC COEFF No. 12
> 26
#             (Bit 23-16)
> f0
#             (Bit 15-8)
> 00
#             (Bit 7-0)
> 00
#             (Bit 31-24) ------------ MSB ADC COEFF No. 13
> 02
#             (Bit 23-16)
> 61
#             (Bit 15-8)
> 00
#             (Bit 7-0)
> 00
#             (Bit 31-24) ------------ MSB ADC COEFF No. 14
> 40
#             (Bit 23-16)
> 02
#             (Bit 15-8)
> 00
#             (Bit 7-0)
> 00
#             (Bit 31-24) ------------ MSB ADC COEFF No. 15
> ff
#             (Bit 23-16)
> fc
#             (Bit 15-8)
> 00
#             (Bit 7-0)
> 00
#             (Bit 31-24) ------------ MSB ADC COEFF No. 16
> ff
#             (Bit 23-16)
> fd
#             (Bit 15-8)
> 00
#             (Bit 7-0)
> 00
#             (Bit 31-24) ------------ MSB ADC COEFF No. 17
> ff
#             (Bit 23-16)
> e5
#             (Bit 15-8)
> 00
#             (Bit 7-0)
> 00
#             (Bit 31-24) ------------ MSB ADC COEFF No. 18
> ff
#             (Bit 23-16)
> a7
#             (Bit 15-8)
> 00
#             (Bit 7-0)
> 00
#             (Bit 31-24) ------------ MSB ADC COEFF No. 19
> ff
#             (Bit 23-16)
> c7
#             (Bit 15-8)
> 00
#             (Bit 7-0)
> 00
#             (Bit 31-24) ------------ MSB ADC COEFF No. 20
> ff
#             (Bit 23-16)
> ce
#             (Bit 15-8)
> 00
#             (Bit 7-0)
> 00
#             (Bit 31-24) ------------ MSB ADC COEFF No. 21
> ff
#             (Bit 23-16)
> fe
#             (Bit 15-8)
> 00
#             (Bit 7-0)
> 00
#             (Bit 31-24) ------------ MSB ADC COEFF No. 22
> fe
#             (Bit 23-16)
> f7
#             (Bit 15-8)
> 00
#             (Bit 7-0)
> 00
#             (Bit 31-24) ------------ MSB ADC COEFF No. 23
> ff
#             (Bit 23-16)
> 46
#             (Bit 15-8)
> 00
#             (Bit 7-0)
> 00
#             (Bit 31-24) ------------ MSB ADC COEFF No. 24
> ff
#             (Bit 23-16)
> 22
#             (Bit 15-8)
> 00
#             (Bit 7-0)
> 00
#             (Bit 31-24) ------------ MSB ADC COEFF No. 25
> ff
#             (Bit 23-16)
> 0f
#             (Bit 15-8)
> 00
#             (Bit 7-0)
> 00
#             (Bit 31-24) ------------ MSB ADC COEFF No. 26
> fa
#             (Bit 23-16)
> 8c
#             (Bit 15-8)
> 00
#             (Bit 7-0)
> 00
#             (Bit 31-24) ------------ MSB ADC COEFF No. 27
> f5
#             (Bit 23-16)
> 08
#             (Bit 15-8)
> 00
#             (Bit 7-0)
> 00
#             (Bit 31-24) ------------ MSB ADC COEFF No. 28
> fd
#             (Bit 23-16)
> 92
#             (Bit 15-8)
> 00
#             (Bit 7-0)
> 00
#             (Bit 31-24) ------------ MSB ADC COEFF No. 29
> f3
#             (Bit 23-16)
> a3
#             (Bit 15-8)
> 00
#             (Bit 7-0)
> 00
#            --------------------------------------------------------------- page 9 is selected
w 30 00 09
#             (Bit 31-24) ------------ MSB ADC COEFF No. 30
w 30 08 03
#             (Bit 23-16)
> b3
Hoping to make an easy transition from the AIC3204 to the AIC3254 with minimal changes, however I understand the miniDSP programming will be another another thing to consider separately.
Thanks in advance, mikm