Hi,
I am using a MEMS Microphone ADMP504 whose output is to be fed to a 12 bit ADC.
ADC i have chose is ADS803.
This ADC has an input capacitance of 20pF (Typical).
Since the MIC's output is only 0.25V peak-peak, i am using LMV1012 pre-amp at the MIC's output.
I am not sure whether this LMV1012 pre-amp can drive the ADC.
I could not find load drive or output capacitance data mentioned in the LMV1012 datasheet.
Could you please help me on this ?
Below is my MIC + Preamp Ckt.
Thanks and regards,
Karthik