Hi,
I am using the TPA3111D1 to drive a predominantly inductive load. The design is based upon the EVM board, with an LC filter, and with -SD and -FAULT linked for automatic recovery. On the datasheet there is no figure for the current threshold at which the over current protection kicks in on this IC. I've successfully managed to get about 2.6Arms at 1kHz sine. The application requires a current of at least 2.4Arms, more would be desirable, obviously I'm running quite close to the limit.
If such a thing exists, I'd like to know a MIN/TYP/MAX figure for the over current threshold on the TPA3111D1. It would also be useful to know if this threshold is higher on the 25W chip, the TPA3112D1.
Regards,
Rowan.