I hoping someone can help me locate an ADC that is capable of sampling stereo analog audio input and produce a 16-bit I2S bus output digital stream. I had been looking at using an ADC developed by Crystal/Cirrus Logic some years ago that is now obsolete. The CS5330 was a small 8pin packaged chip that supported stereo analog audio input but produced an 18-bit size left/right channel words. I need something that specifically only does 16-bit. I prefer a small chip package and supports just I2S (don't need SPI, I2C, etc).
If there isn't one specific TI ADC that can do this is there one that comes close and can be made to interface to a single I2S bus. And if it requires a host to configure it that I can interface using a GPIO style port interface.
Appreciate any suggestions and help that can be given on this subject.
Regards,
Glenn Bruner
CA Polytechnic State Univ.