Hello Texas!
I'm hearing a, however swiftly decaying, white noise when powering up the TAS5706 EVM2 via the !pdn pin. The noise is high freq and sounds like "PFZZzzzz" everytime the !pdn is asserted. The board is configured in BTL mode and so could this be due to that the jumper-bypassed 470uF capacitors (C33 - C36) somehow anyway de-charging or what gives?
Main question is, will I be experience the same noise in a production BTL model that would not have these capacitors at all?
Thanks!
Hanns
Non-Texan but Scanian (which is pretty much the same over here)