Hello: I am passing along these inquiries from my customer:
>>>> For single ended (RCA) inputs, I want to make sure that there are no issues with using the TAS3204 ADC in single ended mode. The EVM uses an extra inverting stage to convert all RCA single ended inputs to differential inputs for the ADC's -- why is that?
The other issue is the TAS3204 registers that control some internal parameters for the ADC's and DAC's (0x13 ~ 0x1D). Without getting into the specifics for each register, I would like to know in general if there is ever any reason to change these registers from the default values. >>>>
regards, G Biner, Arrow FAE LA