Good Day,
I've developed an audio amplifier using the TPA3113D2 and am experiencing some issues with crosstalk between the left and right channels. The amplifier is being fed from two single-ended sources (one at each IN+), with each IN- impedance matched, as suggested in the application note. The outputs are composed of 33uF ferrite-core inductors and 1uF capacitors for the LPF, feeding 8-Ohm loads.
My layout appears to be rather sound, but I am experiencing higher-than-expected crosstalk. The crosstalk presents itself as a 2nd-order harmonic at -40db on the opposite channel to which I am feeding the audio. So for example when I feed 1kHz into the Left side, I see distortion with a main component of 2kHz on the right side, attenutated by about 40dB, and vice vera if I feed the audio into the Right channel.
I have poked around the board with a scope, and have verified that the following:
a) No crosstalk/output frequencies are present in the supply rails or at the supply pins for the TPA3113D2
b) No crosstalk frequencies are present at the input pins for the adjacent channel (feeding audio into left IN+, no crosstalk at right IN+)
c) Crosstalk frequencies are present at the amplifier outputs.
From this, it appears as if the crosstalk is localized to within the TPA3113D2, but that seems incorrect, given the info on the datasheet. Nothing is being over-driven, and I believe I have followed all of the recommendations in the design note, so I am at a loss to understand why the crosstalk performance is so low.
Any help will be greatly appreciated.
Regards,
Matthew