I cannot get my SPDIF signal to lock with PCM2902. I can use SPDIF signal with other equipment but cant get it to lock with my hardware with the PCM2902 what is the tolerance of the PLL in the PCM2902 or is it possibly another issue.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I cannot get my SPDIF signal to lock with PCM2902. I can use SPDIF signal with other equipment but cant get it to lock with my hardware with the PCM2902 what is the tolerance of the PLL in the PCM2902 or is it possibly another issue.
Stuart,
Can you check to see if the S/PDIF data being sent has an asserted "copyright" bit or not? If it is copyrighted then the PCM2902 will automatically select the ADC as the input source.