I'm using ALSA Linux driver, that support tlv320aic3x family.
I see that this driver writes to the following registers
Page 0/Register 45: Reserved Register
Page 0/Register 48: Reserved Register
Page 0/Register 52: Reserved Register
Page 0/Register 55: Reserved Register
Page 0/Register 59: Reserved Register
Page 0/Register 62: Reserved Register
Page 0/Register 66: Reserved Register
Page 0/Register 69: Reserved Register
Page 0/Register 79: Reserved Register
Page 0/Register 80: Reserved Register
Page 0/Register 83: Reserved Register
Page 0/Register 87: Reserved Register
Page 0/Register 90: Reserved Register
Should I really remove these writes from the driver or can I think that this unwanted settings are not introducing problems in the codec?
Thx,
Raffaele