This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USB-MODEVM possible issue.

I am using the Purepath GDE and it works great.  At least until I remove the USB connection and reconnect.  The MODEVM seems to require reprogramming with a reset or power cycle.  I need to provide the unit with a power source as a bit of a demonstration unit and I need to do this without sending a laptop.  Is there a bit that needs to be set to keep it from dumping the memory or is is just not auto starting when power is applied?

Thanks.