Hey!
I'm studying electronic and communication systems and i'm getting prepared
for my bachelor thesis this days witch will start in about two months.
I want to build a two channel audio-dj-mixer with dsp. Maybe i will use your
TLV320AIC3256EVM-U Evaluation Module for this, because there are not many
affordable boards with this amount of audio inputs and outputs.
Link to Board: http://www.ti.com/tool/tlv320aic3256evm-u
At the moment the board seems to be a good affordable solution, but i do have a few questions left.
I want to connect the user interface to the DSP by I²C or SPI. On the DSP i need some volume controls and a parametric 3-band equalizer for each channel witch also get's triggered from I²C (or SPI). At the moment i'm missing an overview what's possible with PurePath Studio.
So, is there such an equalizer available in PurePath Studio? Are the controls of the GDE Blocks accessible from I²C or SPI?
How are the inputs of ADC-channel 2 (IN2_L IN2_R) realized on the Board? I see that there's no connector like channel 1, are there some kind of soldering-pads or any other kind of connectors?
Thanks and regards!
Christian Kleiner