This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Is there any way to read internal volume register from the PCM2705 using SPI?

Other Parts Discussed in Thread: PCM2705

 It appears an HID status register exists but no information in the datasheet that would allow external reading of volume level.  Is there a way to read the static volume from a PCM2705 using SPI? 

 

  • Hi Dale,

    No, it is not possible to directly read the internal volume register on the PCM2705 using SPI.  The SPI 's functionality is limited to being used to write HID-type commands (volume up, volume down, mute, etc.) to the PCM2705, or for programming the device's descriptor.

     

    Regards,

    Nick