Hello,
we are currently in the process of evaluating hardware for our design and we have been looking at the TAS5727 DAC+Class D amplifier for our design. We have purchased an evaluation kit and are interfacing it to our own hardware. With the TI software we are able to produce sound through the ADC so all components seem to work.
The reason we chose the TAS5727 is that in the datasheet it is stated that:
"The clock section uses MCLK or the internal oscillator clock (when MCLK is unstable, out of range, or absent) to produce the internal clock (DCLK) running at 512 times the PWM switching frequency".
This made use believe that we could actually could get away with just connecting SCLK, LRCLK and SDIN and the amplifier could work (no MCLK connection required).
Is this assumption correct and will the internal oscillator generate MCLK or does the amplifier really need MCLK connected to properly fuction?
Best regards,
Oane