Hi, I'm designing a power amplifier which uses PGA2320/2311 as input attenuator. This device is controlled by a USB SPI bridge, and here is the question. What is the relationship between VA and VD? Can I power up VA without VD or vice versa? How will this device behave with VA but without VD? Will it mute or remain previously programmed value?(My senario is a device connects to an permanent analog supply and a hot-pluggable USB power. The VA is always on, but the VD is not guaranteed. The VD is also possible to be on without VA, where the device is not powered, but the USB is plugged.)