Hello~
According to DRV603EVM & DRV632EVM, it is using the 16V voltage rating for the Charge Pump Flying CAP.
Is the 16V voltage rating mendatory??
If the VDD is 3.3V, Can I use 10V or 6.3V rating instead of 16V voltage rating for the Charge Pump Flying CAP??
Thanks... C.W. :)