Hello,
I would have your comment about the use or the behavior of the TPA2005D1.
My test configuration is the following: a MCU generates 2 differents PWM audio signals (150KHz PWM frequency), each one applied to a 1µF-150KOhms RC network (decoupling capacitor in series with gain resistor) connected to each IN- and IN+ inputs pins. A speaker connected between VO+ and VO- finally gives the mixed audio signals.
As you can see I'm not using any RC low-pass filter to smooth the PWM signals before application to the audio amplifier, but the TPA2005D1 works well. If I insert a RC low-pass filter (Fc < 20KHz), I just got a sound a little bit noisy (with a sound quality enough for my application).
I'm finally surprised to see that the LPF is not mandatory, and that the TPA2005D1 finally behaves normally.
Is this configuration of use finally acceptable, or do you see any possible drawbacks or risks ?
I greatly thank you for your answer.
Best regards,
Joël