This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AIC3254EVM without USB data connection

Hello

I have managed to get my AIC3254EVM working and can edit and program the various DSP features using the GDE. It keeps working and streaming audio as long as it is still plugged into the PC USB port. 

I would like to be able to use the EVM in its current programmed state away from the PC by just powering up the board with 5V. However, when I disconnect the EVM from the PC and then power it back up with 5V, it no longer works and streams audio. I am guessing the device is reset?

Is there any way to keep the device programmed so it returns to the same state after you re-apply power? I have tried clicking "write state" and "disconnect" in the build options of the GDE. Surely this is possible?

Please let me know

Thanks

David