Hi,
Iam working on integrating TLV320AIC10 codec with AMBE2000 vocoder. I have configured TLV320AIC10 to work at SCLK of 2.048 MHz, FS is 8kHz. Input is selected as AURXM and AURXFP through configuration. For validating TLV320AIC10, I wanted to test it in Digital loopback. I tried to do so by first configuring it in digital loop back mode (D7=1 and D6=0 of control register 3). Then I checked the audio output at OUTM and OUTP. Nothing is heard. What could be the issue. I also tried by shorting DIN and DOUT pins physically. Please help me ouyt with this situation.
Thanks and regards,
Srikanth.