Other Parts Discussed in Thread: TAS5630
Hello,
If I were to drive the TAS5630 input using a 50/60 Hz sine wave and use a transformer to step-up the voltage to 230Vrms, i.e. use it as the power stage of a sine wave inverter, then can the TAS5630 'built-in closed-loop' be able to regulate the power from no-load to full-load. I understand that since there will be a 50/60 Hz current flowing through the o/p transformer, it would very bulky. I just thought of knowing more about the chip with regards to changing loads, even if it not a typical audio scenario.
Thanks in advance.
Ravindra.