Hi the
I nticed that precious post (http://e2e.ti.com/support/amplifiers/audio_amplifiers/f/6/t/28843.aspx) specifies how to setp the the TAS5162 in the event only one half of the outputs are being used. I have a similar situation wtih the TAS5615 where Ionly plan on using the A&B outputs and not the C&D outputs.
Would it be safe to say that I can connect things in the same way specified in the in the above link which specifies the following:
Connect the PWM input of the unused 1/2 bridge to one of the driven PWM inputs; otherwise, the input activity detector will cause the whole device to shutdown. Then, add the bootstrap cap, BST_x to OUT_x of the unused channel. Finally, connect the PVDD_x (PVDD pin of the unused 1/2 bridge) to GND (ground). The output of the unused channel can then be left floating.
Thanks
tB