Hi, after mi last mesage We finish other proyect and I will satrt to work with the pga4311 to made a gain control of our desing.
After reading the data shhet I have some easy questions, to conect at the output of each chanels of the atenuator, Iread taht is possible to conect transducers with impedance lower than 600ohms. I think taht the op inside made the impedance conversion. I think taht is possible to conect the transducer directly, is that correct??
Other thing, with this device we will have a dinamic range of 127db, we need 120dB but we need another extrernal +-10dB to fit a calibration the spl db (sound presure levels) with HL db (hearing level db) there is a special iso correction values.
The imput will be an analog audio.
In case taht we use 2 chanels one for the ateanution and the output to the imput of other for the other for the calibratión factors, I think it will be better sound with only one adc and dac conversión. What do you think about it? Any component recomendation ?
And for finish, Is possible to now the specting year to manufactury stop of the pga4311? is good for a new desing??
Best regards abd thaks for all
Luis