Other Parts Discussed in Thread: PCM5310
Our customer has been evaluating PCM5310 on their own designed H/W, and reported that the line output signal was clipped at 3.3Vpp under below conditions.
1. Signal pass:
AIN2L → PCM5310(ADC)→(I2S)→ DSP → (I2S)→ PCM5310(DAC) → LO1L
2. ADC input level: 2V_rms Sine wave
3. Analog input gain = 0dB, ADC attenuation = 0dB, DAC attenuation=0dB
4. In case of Analog input = 2V_rms (5.6 Vpp), LO1L output of both upper side and bottom side is clipped at 3.3Vpp.
5. Output signal is not clipped when decreasing analog input signal level to 3.3Vpp.
6. Confirmed the power supplies.
VREFAD1 (62pin) = VCOMAD(64pin) = VCOMDA(25pin) =1.64V
7.The register setting is the same as [Table 8. Recommended Register Settings When Powered On (continued)] of datasheet.
Does anyone have any suggestion or advice for solving this problem?
Thanks in advance.
Regards,
Toshi