This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM5310 pop noise when power on/off

Other Parts Discussed in Thread: PCM5310

Hi,
My customer has a question below.

According to the datasheet of PCM5310,   ramp up/down time for the analog output can be changed through the register setting (Register 18, PDTM[2:0]).

For reducing pop noise when power is on or off, customer sets  [100] to REG18 PRTM[2:0].
And this value is expected 1000 ms for a ramp up time of power-up, and 2000 ms for a ramp down time of power-down. However the result is about 300ms for both cases.
A 1.0-μF capacitor is connected to VCOMAD and VCOMDA pins.

Is there  any method of extending the ramp up/down time?

Regards,
Toshi